Other Parts Discussed in Thread: TM4C1294NCPDT
Dear Sir.,
We need the High performance Tiva microcontroller as per the following specifications.
We are going to developing the Industrial Textile Machinery with High speed and High performance,
Already we are using TIva TM4C1294NCPDT & KCPDT microcontrollers.
But this controller currently not fit to our requirement.
Required Specification:
1. High performance 32 Bit and DSP with FPU .
2. 700MHZ CPU to 800 MHZ core clock.
3. 1MB RAM and 2MB Flash Memory.
4.Minimum 208 pin LQPF
5.2x8 Channel ADC
6. 2x8 Channel DAC
7. Timer with PWM support
8. UART,SPI,I2C,CAN,Ethernet MAC10/100 MBit,USB2.0 HS/FS(2 COUNT)
9. 8 Channel DMA
10. Real Time operating system sporting.
11. RTC(Real Time Clock)
12. EPROM(4-16 Mbit)
Please suggest the microcontroller with above specifications.