Part Number: MSPM0G3105
Other Parts Discussed in Thread: UNIFLASH, MSPM0G3507
Hello,
while debugging my firmware with XDS110 in CCS v.12.4.0 suddenly I receive this message:
Error connecting to the target: (Error -6305) PRSC module failed to write to a router register. (Emulation package 9.12.0.00150).
After I get this, no matter what I do, I can't access anymore the MCU because I always get this message.
I've tried to access the MCU also over UniFlash programming utility but I always get this message.
Of course I've tried to switch off and on the board power supply but it doesn't help.
It seems like the MCU is locked into a particular state or condition that doesn't allow the debugger to recovered it anymore. Is this possible? If yes, what might be the cause?
This problem happened quite often since I've started working on the firmware and I've already locked 3 boards.
Best Regards,
Nicola