Part Number: AM2634-Q1
Should the crystal oscillator ground be connected to VSS?
Or connect to VSSA?
Datasheet: In Table 6-1 of SPRSP74, the POWER column for XTAL_XI and XTAL_XO is VDDS_OSC.
However, "VDDS_OSC" is not written anywhere else.
I think VDDS_OSC is different from VDDA18_OSC_PLL.
Hardware Design Guide: SPRABJ8 3.4 Crystal Placement and Routing states "A ground ring shorted to the local VSS plane should be placed adjacent".
However, looking at the picture, GND is also connected to the VSSA's BGA Pads.
Also, what is a "ground ring"?
Japanese memo
水晶発振器のグランドはVSSに接続するのか?
それともVSSAに接続するのか?
データシート:SPRSP74の表6-1ではXTAL_XIとXTAL_XOはPOWERの欄がVDDS_OSCとなっている。
しかし「VDDS_OSC」はその他の箇所には記載されていない。
VDDS_OSCはVDDA18_OSC_PLLと別物と考えている。
ハードウェアデザインガイド:SPRABJ8 3.4 Crystal Placement and Routingでは「A ground ring shorted to the local VSS plane should be placed adjacent」と記載されている。
しかし絵を見るとGNDはVSSAのBGA Padsにも接続されている。
それと「ground ring」とは何ですか?