Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1310: Changes required to remap SPI pins

Part Number: LAUNCHXL-CC1310
Other Parts Discussed in Thread: CC1310, SYSCONFIG

Greetings

I am trying to remap the default SPI0 pins to the following mapping:

#define CC1310_LAUNCHXL_SPI0_CS          IOID_25
#define CC1310_LAUNCHXL_SPI0_MISO      IOID_1
#define CC1310_LAUNCHXL_SPI0_MOSI      IOID_0
#define CC1310_LAUNCHXL_SPI0_CLK        IOID_2

How is this done? I am aware of the spiCC26XXDMAHWAttrs struct in the LAUNCHXL.C, where changes have to be made to the members of the strruct that specify the pins for each function, but not sure if changes are required elsewhere. I have referred to a older post but most of the links which have been provided to the OP in that post are not accessible now, links which indicate changes need to be made to the ioc.h file. Are there changes required in that file?

Regards

Suvashan