In TRM "Literature Number: SPNU489B", PBIST chapter, in table 6-1, i have the following questions:
1. What is ESRAM ? Is it the 160KB SRAM (address: 0x0800 0000-0x0822 7FFF) ?
2.
what is sigle/two port RAM? what does sigle/two mean ?
3. how to use the RGS/RDS value ? In the table 6-1,in RGS/RDS column, "5/0..5" and "1/0..2", what does it mean ?
And other questions continue,
4. In many registers, e.g., in FSRF0 and FSRF1, it metions port 0 and port 1, what is port 0 and port 1 ? does it have any relationship with single/dual port ?
5. what should do in these two function "memoryPort0TestFailNotification" and "memoryPort1TestFailNotification"? these two function are called in assembly language "_memoryTest_", which is generated by HALCoGen and called in function "_c_int00()".
6. how to test PBIST functionality ? how to make it fail ? which errors will cause PBIST test fail ?
7. Besides TRM document, Is there any other documents describe PBIST module? can you send to me?
thanks very much.