This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2634: CCS Clock Cycles Do Not Match R5F Core Frequency

Part Number: AM2634

Hello,

Using the rti_led_blink_am263x-cc_r5fss0-0_nortos_ti-arm-clang project out of the box with the EVM, the LED blinks ten times, once every 1s.

If I put the breakpoints here....

Then at R5F clock frequency of 400MHz, 10s should be 4,000,000,000 clock cycles give or take.

To reduce error, I did ten trials:

3,177,097,230

3,494,932,568

3,197,364,068

3,295,250,550

3,296,489,980

3,287,200,992

3,172,247,852

3,342,880,474

3,168,000,196

3,196,881,434

The average is 3,262,834,534 which means the number of clock cycles is ~20% lower than expected. There's a few possible explanations for this:

1) The CCS Clock Cycle measurement doesn't work correctly.

2) The R5F core is stopping or sleeping for 20% of the time.

3) The R5F core clock frequency is ~362MHz not 400MHz as advertised by the GEL file.

4) Something else.

Could you help me understand the cause of the discrepancy please?

This matters because I want to measure the real time for execution in my actual project using the clock but at the moment, I can't rely on its results.

Thank you.