Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129ENCPDT: SD card hardware and communication

Part Number: TM4C129ENCPDT

Hi,

I have a board with a TM4C129 uC. Now I would like to use a micro SD card as memory. I am currently setting up the hardware.

I found the DK-TM4C129X board with SD card function on the web. Now I see that only one SD card holder (2908-05WB-MG) is used here and is connected to the SPI interface of the uC.

Is that really all, I thought that a driver module is needed here. Could you help me with this?