Part Number: LAUNCHXL-CC1310
Other Parts Discussed in Thread: CC1310
Greetings
I am attempting to write functions to condense SPI communication between a CC1310 and a LPS22HB pressure sensor. Instead of continuously initialising parameters etc., I would like to have a function for r/w functions using SPI.
For my SPI_Write function:
bool SPI_Write(SPI_Handle spi_handle, SPI_Params spi_params,
SPI_Transaction spi_transaction, uint8_t size,
uint8_t *txBuffer)
{
SPI_Params_init(&spi_params);
spi_params.transferMode = SPI_MODE_BLOCKING;
spi_params.bitRate = 10000000;
spi_params.dataSize = 8;
spi_handle = SPI_open(0, &spi_params);
if (!spi_handle) {
// Error opening SPI
return false;
}
spi_transaction.count = size;
spi_transaction.txBuf = txBuffer;
spi_transaction.rxBuf = NULL;
if(!SPI_transfer(spi_handle, &spi_transaction))
{
return false;
}
SPI_close(spi_handle);
return true;
}
For my SPI_Read function:
bool SPI_Read(SPI_Handle spi_handle, SPI_Params spi_params,
SPI_Transaction spi_transaction, uint8_t size,
uint8_t *rxBuffer)
{
SPI_Params_init(&spi_params);
spi_params.transferMode = SPI_MODE_BLOCKING;
spi_params.bitRate = 10000000;
spi_params.dataSize = 8;
spi_handle = SPI_open(0, &spi_params);
if (!spi_handle) {
// Error opening SPI
return false;
}
spi_transaction.count = size;
spi_transaction.txBuf = NULL;
spi_transaction.rxBuf = rxBuffer;
if(!SPI_transfer(spi_handle, &spi_transaction))
{
false;
}
SPI_close(spi_handle);
return true;
}
In turn, my driver for the LPS22HB consists of:
SPI_Transaction LPS22HB_SpiTransactionHandle;
SPI_Handle LPS22HB2_SpiHandle;
SPI_Params LPS22HB_SpiParams;
#define TOGGLE_CS GPIO_write(Board_GPIO_TEST_DIO25, 0)
#define RELEASE_CS GPIO_write(Board_GPIO_TEST_DIO25, 1)
static void LPS22HB_Mem_Write(uint8_t reg, uint8_t *dataW, uint8_t size)
{
uint8_t spiReg = reg;
TOGGLE_CS; //sets the CS low
SPI_Write(LPS22HB_SpiHandle, LPS22HB_SpiParams, LPS22HB_SpiTransactionHandle, 1, &spiReg);
SPI_Write(LPS22HB_SpiHandle, LPS22HB_SpiParams, LPS22HB_SpiTransactionHandle, size, dataW);
RELEASE_CS; //sets the CS high
}
static void LPS22HB_Mem_Read(uint8_t reg, uint8_t *dataR, uint8_t size)
{
uint8_t spiBuf[1] = {0};
spiBuf[0] = reg | 0x80;
uint8_t i;
TOGGLE_CS; //sets the CS low
SPI_Write(LPS22HB_SpiHandle, LPS22HB_SpiParams, LPS22HB_SpiTransactionHandle, 1, spiBuf);
SPI_Read(LPS22HB_SpiHandle, LPS22HB_SpiParams, LPS22HB_SpiTransactionHandle, size, dataR);
RELEASE_CS; //sets the CS high
}
I am then trying to read the chip_id ("Who am I" of the sensor), which should be 0xB1, using the following code segment:
LPS22HB_Mem_Read(0x0f, ui8dummy, 1);
uint8_t ui8dummy[2]
if(strcmp(ui8dummy, "D") != 0)
{
return false;
}
When I read the chip-ID, I get zero, when I expect a value of 0xb1, given by the datasheet. I have debugged the SPI R/W code extensively. I have added breakpoints to the SPI_W/R functions and can guarantee that no errors are raised (the functions do not return false). I am using a software chip-select, given by the "toggle" and "release" macros. I can confirm my CS and clock works, as I've checked this on a scope. I am using the uartEcho example from the CC1310 SDK of version 20.02.07.
Are there any glaring errors in my driver for it to not work?