Part Number: TMS570LS0432
Other Parts Discussed in Thread: HALCOGEN
Hi TI Community,
I am doing a program to turn on a led in TMS570LS0432 launch pad, I found one YouTube video https://www.youtube.com/watch?v=tsVmpH6Pm2U here i did same thing as per video, but CCS is throwing errors that
"../source/sys_main.c", line 90: error #148: declaration is incompatible with "void gioNotification(gioPORT_t *, uint32)"
i have included gio.h also pls find code below:
/* USER CODE BEGIN (0) */
#include "het.h"
/* USER CODE END */
/* Include Files */
#include "sys_common.h"
#include "gio.h"
/* USER CODE BEGIN (1) */
/* USER CODE END */
int main(void)
{
/* USER CODE BEGIN (3) */
// set port pins to output
//gioPORTA.DIR |= (1U << 2);
gioSetDirection(hetPORT1, 0xFFFFFFFF);
while (1)
{
// Turn on the LED
//gioPORTA.DSET = (1U << 2);
gioSetBit(hetPORT1, 5, 1); // GIOA2 //on 5th pin led present
}
/* USER CODE END */
// return 0;
}
/* USER CODE BEGIN (4) */
void gioNotification(int bit)
{
return;
}
void esmGroup1Notification(int bit)
{
return;
}
void esmGroup2Notification(int bit)
{
return;
}
please help me to figured out this I am new to Taxes instruments controllers.
Best Regards,
Tyagi