This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2634: gpmc - freertos

Part Number: AM2634

hi

Implemented gpmc0 in noos mode.
Put the value directly into the register and do the desired action.
An error occurs while implanting the gpmc implemented in noos mode from freetos.
Go to TaskP_loadGet(), I don't know why.
What should I do?

  • Hi Kwon,

    Where did you initialize the GPMC PSRAM (the only GPMC mode which AM263x MCU+ SDK 09.01.00.44 currently supports)?

    You cannot use the memory area starting at 0x68000000 until the GPMC initialization is done.

    Best regards,

    Ming

  • hi 

    I set it up like an image.
    I did it at freertos.
    error occurs in freertos.
    It works well with noos.

  • Hi Kwon,

    Which AM263x MCU+ SDK are you using? 09.00.00 or 09.01.00?

    Best regards,

    Ming

  • hi

    sdk 09.01.00.41

  • Hi Kwon,

    The AM263x GPMC initialization is the same between the NORTOS and FreeRTOS. It is done using the syscfg (in ti_drivers_config.c): System_init -->  GPMC_init (passing parameters through gGpmcConfig).

    One thing you can try is to comment out the following code:

    pSrc = &buff[0];
    pDes = (uint16_t *)0x68000000;
    *pDes = *pSrc;

    If the error is gone, then it means your GPMC initialization is not completed correctly. You can check the 0x68000000 with Memory Browser in CCS. It should show that the memory area is not available. 

    If that is the case, then two things can go wrong:

    1. The MPU setting for GPMC memory space is not done correctly.

    2. The GPMC initialization is not done correctly.  

    You can refer to gpmc_psram_io_am263x-cc_r5fss0-0_nortos_ti-arm-clang for both items.

    I tried your test case based on the modified empty_am263x-cc_r5fss0-0_freertos_ti-arm-clang (mimic gpmc_psram_io_am263x-cc_r5fss0-0_nortos_ti-arm-clang) on the AM263x LP without the PSRAM daughter card. Th example runs to data abortion with the above code (accessing GPMC memory)  

    Best regards,

    Ming