We have been using Code Composer Studio 10.1 for a while, and recently explored upgrading to CCS 12.6.
In CCS 12.6, the Navigate menu (which was also available via a right mouse click), appears to no longer support Open Declaration, Open Type Hierachy, etc, features which we often used and found to be very helpful. Is there a configuration setting that would allow these features to become available again, or are they permanently removed?