Part Number: MCU-PLUS-SDK-AM263X
Other Parts Discussed in Thread: SYSCONFIG
I am trying to understand ePWM registers. There is a Register Addendum manual (spruj42d.pdf) that gives a definition for the AQCTL register, associated with a memory offset of 0x20 (Table 3-704). In the SDK, this is defined in the file cslr_etpwm.h as follows:
#define CSL_EPWM_AQCTL (0x00000020U)
My question is what about the later registers, defined in this same file as:
#define CSL_EPWM_AQCTLA (0x00000080U)
#define CSL_EPWM_AQCTLA2 (0x00000082U)
#define CSL_EPWM_AQCTLB (0x00000084U)
#define CSL_EPWM_AQCTLB2 (0x00000086U)
What is their definition?
I ask because I have received some code that is setting the location (CONFIG_EPWM0_BASE_ADDR+CSL_EPWM_AQCTLA+2) to values such as
| 0x0012 | 0x0048 | 0x0840 | 0x0060 | 0x0090 | 0x0600 | 0x0900 |
And some of these are setting what would be reserved bits or bits that only matter if SHDWAQxMODE is set to 1 while setting SHDWAQxMODE to 0.