This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: Can I use exactly the same N2HET code for my TMS570LC4357 that was generated for TMS570LS3137?

Part Number: TMS570LC4357
Other Parts Discussed in Thread: TMS570LS3137, HALCOGEN,

I wrote the TMS570LS3137 N2HET code ~7 years ago, and I am struggling to find the origin of my own code, so I have 2 questions:

1. Is there an app-note or example c-code that uses the hetp.exe to create the .het file? I don't remember using HALCOGEN for this specific code, and my HalCoGen is looking for an external C/H file to import, so there must be example code somewhere?

2. It looks like the TMS570LC4357 is identical to the TMS570LS3137, but I am visually comparing TRMs -- are they identical (is the IP the same), and the same hetp.exe works for both?

Thanks,

Jim