Part Number: MSPM0L1105
Team,
my customer needs a very small solution size. They have some questions regarding the circuitry shown in Application Note „MSPM0 L-Series MCUs Hardware Development Guide“ (SLAAE75A) and potential to reduce size:

- To what value can the 10uF capacitor at VDD be reduced to a minimum?
- Can only one capacitor be used instead of the two capacitors on VDD?
- With STM controllers, it is possible to configure the NRST pin as GPIO. Thus, the resistor and the capacitor at NRST are eliminated.
Is this also possible with TI's µCs? - The 100kOhm is optional to improve the accuracy of the internal resonator, right?
- Can you buy TI programmed µCs? We set the program and TI programs and ship to the EMS.
What would this cost per µC?
Best regards