Part Number: MSPM0G3507
Hello,
I'm unable to calculate the right temperature value. I have the following input values:
- ADC digit is 1834
- ADC reference voltage is 1.4V
- DL_SYSCTL_getTempCalibrationConstant() returns 752
-
TEMP_TS_COEF_mV_C is -571.42
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSPM0G3507
Hello,
I'm unable to calculate the right temperature value. I have the following input values:
Hi Sebastian,
I am not sure 18℃ is the definitely correct in your case. But this data seems to be reasonable for the temperature of the chip itself.
Maybe you can use a thermometer to actually measure the temperature inside the chip and compare it.
"Maybe you can use a thermometer to actually measure the temperature inside the chip and compare it."
How would this work? As a semiconductor engineer I am dying to know.
While in absolute terms 18C is a reasonable number, if the ambient is 22, unless the chip is violating the 2nd law, it is impossible for it to be *cooler* than its environment.
I note that there are no accuracy specs given, so I suspect that there is a 3-4 degree error possible.
Sorry, I mean use thermal imager not thermometer.
Actually, we have recently been retrimming the temperature sensor internally, thanks for the news that gave us.