Part Number: TMDSCNCD263P
Other Parts Discussed in Thread: SYSCONFIG, UNIFLASH
Hello,
I have tried to use two enet examples from mcu_plus_sdk_am263px_09_01_00_20 but neither are able to get an IP address via DHCP. For example: enet_lwip_cpsw_am263px-cc_r5fss0-0_freertos_ti-arm-clang
The Terminal output is:
==========================
ENET LWIP App
==========================
EnetAppUtils_reduceCoreMacAllocation: Reduced Mac Address Allocation for CoreId:0 From 4 To 2
Link Status Changed. PHY: 0x0, state: up
EnetPhy_bindDriver:1828
PHY 0 is alive
Starting lwIP, local interface IP is dhcp-enabled
[LWIPIF_LWIP] NETIF INIT SUCCESS
Host MAC address-0 : 70:ff:76:1f:60:20
[LWIPIF_LWIP] Enet has been started successfully
[0]status_callback==UP, local interface IP is 0.0.0.0
UDP server listening on port 5001
Cpsw_handleLinkUp:1629
MAC Port 2: link up
link_callback==UP
5. 44s : CPU load = 1.17 %
10. 44s : CPU load = 0.98 %
IP address is always 0.
I am using the same cable that was plugged into my oscilloscope where I could access its http server. So cabling and router DHCP are working fine.
The RJ45 LEDs indicate as follows:
Left hand (closest to USB-C) : steady yellow.
Right hand : intermittent green.
Please can you confirm if any of the examples are running correctly out of the box on TMDSCNCD263P.
Thank you.