Part Number: TM4C1294NCPDT
I am using lwiopts file for tcp ip communication . following are the line of code for full duplex communciation.
#if !defined(EMAC_PHY_IS_EXT_MII) && !defined(EMAC_PHY_IS_EXT_RMII)
#define EMAC_PHY_CONFIG (EMAC_PHY_TYPE_INTERNAL | EMAC_PHY_INT_MDIX_EN | \
EMAC_PHY_AN_10B_T_FULL_DUPLEX)
Issues observed:
Ethernet is not working with full duplex managed switch. However it works with half duplex code.
Please help.