Hello Team,
In the launch pad of the MCU MSP432E401YTPDTR, we have an onboard debugger based on the controller TM4C129ENCPDTI3R.
The TM4C129ENCPDTI3R will be converting the USB to JTAG format to flash the MSP controller.
Do we need TM4C129ENCPDTI3R in our own board?
I hope we can use an XDS100 to flash the MSP controller or the launchpad can flash the custom board via SWD or JTAG.
And we can perform all the debugging functions through JTAG just like we can do it via TM4C129ENCPDTI3R
If we are planning to include the TIVA controller also in our board due to various reason for flashing and debugging purpose only (like in the case of launchpad), will TI provide the firmware in the TIVA MCU?
Can anyone please confirm the firmware for the debugger on the launchpad for the TM4C129ENCPDTI3R is open source or not?.
If yes please send the code.
Looking for your reply