Part Number: TM4C1294NCPDT
Hi,
I am sending the data over UART and I am checking it onto the terminal. while receiving the data I am getting the garbage value , i am not getting where I am making the mistake.
When I am putting the brakpoint at loine number 534 and 578 the data is receiving as desired.
#0000#0fff
#0002#0fff
#0000#0fff
#0000#0fff
but when we removed the breakpoint i am getting the garbage value.
#0001########
#######
##0002#0fff
#0000####f##########
###0001#0fff
#0002########
###
###f##0000#0ffc
#0001####f##########
###0002#0fff
#0000########
#######f##0000#0fff
#0003####f##########
###0001#0fff
#0000########
#######f##0001#0fff
below is my Code.
#include <stdbool.h>
#include <stdint.h>
#include <string.h>
#include <stdio.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_emac.h"
#include "inc/hw_udma.h"
#include "inc/hw_adc.h"
#include "driverlib/flash.h"
#include "driverlib/interrupt.h"
#include "driverlib/gpio.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/rom.h"
#include "driverlib/adc.h"
#include "driverlib/uart.h"
#include "driverlib/pin_map.h"
#include "driverlib/timer.h"
#include "driverlib/udma.h"
#include "drivers/pinout.h"
#include "utils/lwiplib.h"
#include "utils/ustdlib.h"
#include "utils/uartstdio.h"
#include "lwip/debug.h"
#include "lwip/stats.h"
#include "lwip/tcp.h"
#include "lwip/inet.h"
//
// The variable g_ui32SysClock contains the system clock frequency in Hz.
//
//*****************************************************************************
uint32_t g_ui32SysClock;
// Definition for ADC buffer size.
//
//*****************************************************************************
#define ADC_SAMPLE_BUF_SIZE 64
#define Channels 2
//*****************************************************************************
//
// The control table used by the uDMA controller. This table must be aligned
// to a 1024 byte boundary.
//
//*****************************************************************************
#if defined(ewarm)
#pragma data_alignment=1024
uint8_t pui8ControlTable[1024];
#elif defined(ccs)
#pragma DATA_ALIGN(pui8ControlTable, 1024)
uint8_t pui8ControlTable[1024];
#else
uint8_t pui8ControlTable[1024] __attribute__ ((aligned(1024)));
#endif
//*****************************************************************************
//
// Global buffers to store ADC sample data.
//
//*****************************************************************************
static uint16_t pui16ADCBuffer1[ADC_SAMPLE_BUF_SIZE][Channels];
static uint16_t pui16ADCBuffer2[ADC_SAMPLE_BUF_SIZE][Channels];
//*****************************************************************************
//
// Each possible state of the fill status for an ADC buffer.
//
//*****************************************************************************
enum BUFFER_STATUS
{
EMPTY,
FILLING,
FULL
};
uint8_t k=0;
//*****************************************************************************
//
// Global variable to keep track of the fill status of each ADC buffer.
//
//*****************************************************************************
static enum BUFFER_STATUS pui32BufferStatus[2];
//*****************************************************************************
//
// The count of uDMA errors. This value is incremented by the uDMA error
// handler.
//
//*****************************************************************************
static uint32_t g_ui32DMAErrCount = 0u;
//*****************************************************************************
//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif
//*****************************************************************************
// User Defined Function Proto
void init_TIMER(void);
//*****************************************************************************
//
// The UART interrupt handler.
//
//*****************************************************************************
void
UARTIntHandler(void)
{
uint32_t ui32Status;
//
// Get the interrrupt status.
//
ui32Status = MAP_UARTIntStatus(UART0_BASE, true);
//
// Clear the asserted interrupts.
//
MAP_UARTIntClear(UART0_BASE, ui32Status);
//
// Loop while there are characters in the receive FIFO.
//
while(MAP_UARTCharsAvail(UART0_BASE))
{
//
// Read the next character from the UART and write it back to the UART.
//
MAP_UARTCharPutNonBlocking(UART0_BASE,
MAP_UARTCharGetNonBlocking(UART0_BASE));
//
// Blink the LED to show a character transfer is occuring.
//
MAP_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, GPIO_PIN_0);
//
// Delay for 1 millisecond. Each SysCtlDelay is about 3 clocks.
//
SysCtlDelay(g_ui32SysClock / (1000 * 3));
//
// Turn off the LED
//
MAP_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, 0);
}
}
//*****************************************************************************
//
// Send a string to the UART.
//
//*****************************************************************************
void
UARTSend(const uint8_t *pui8Buffer, uint32_t ui32Count)
{
//
// Loop while there are more characters to send.
//
while(ui32Count--)
{
//
// Write the next character to the UART.
//
UARTCharPutNonBlocking(UART0_BASE, *pui8Buffer++);
}
// UARTCharPutNonBlocking(UART0_BASE, '\n');
}
//*****************************************************************************
//
// The interrupt handler for uDMA errors. This interrupt will occur if the
// uDMA encounters a bus error while trying to perform a transfer. This
// handler just increments a counter if an error occurs.
//
//*****************************************************************************
void
uDMAErrorHandler(void)
{
uint32_t ui32Status;
//
// Check for uDMA error bit.
//
ui32Status = uDMAErrorStatusGet();
//
// If there is a uDMA error, then clear the error and increment
// the error counter.
//
if(ui32Status)
{
uDMAErrorStatusClear();
g_ui32DMAErrCount++;
}
}
//*****************************************************************************
//uDMA Configuration
void uDMAConfigure(void)
{
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);
uDMAEnable();
//
// Point at the control table to use for channel control structures.
//
uDMAControlBaseSet(pui8ControlTable);
//
// Put the attributes in a known state for the uDMA ADC0 channel. These
// should already be disabled by default.
//
uDMAChannelAttributeDisable(UDMA_CHANNEL_ADC0,
UDMA_ATTR_ALTSELECT | UDMA_ATTR_HIGH_PRIORITY |
UDMA_ATTR_REQMASK);
//
// Configure the control parameters for the primary control structure for
// the ADC0 channel. The primary control structure is used for the "A"
// part of the ping-pong receive. The transfer data size is 16 bits, the
// source address does not increment since it will be reading from a
// register. The destination address increment is 16-bits. The
// arbitration size is set to one byte transfers.
//
uDMAChannelControlSet(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT, UDMA_SIZE_16 |
UDMA_SRC_INC_NONE | UDMA_DST_INC_16 | UDMA_ARB_1);
//
// Configure the control parameters for the alternate control structure for
// the ADC0 channel. The alternate control structure is used for the
// "B" part of the ping-pong receive. The configuration is identical to
// the primary/A control structure.
//
uDMAChannelControlSet(UDMA_CHANNEL_ADC0 | UDMA_ALT_SELECT, UDMA_SIZE_16 |
UDMA_SRC_INC_NONE | UDMA_DST_INC_16 | UDMA_ARB_1);
//
// Set up the transfer parameters for the ADC0 primary control structure
// The mode is set to ping-pong, the transfer source is the ADC Sample
// Sequence Result FIFO 0 register, and the destination is the receive
// "A" buffer. The transfer size is set to match the size of the buffer.
//
uDMAChannelTransferSet(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT,
UDMA_MODE_PINGPONG,
(void *)(ADC0_BASE + ADC_O_SSFIFO0),
&pui16ADCBuffer1, ADC_SAMPLE_BUF_SIZE * Channels);
//
// Set up the transfer parameters for the ADC0 primary control structure
// The mode is set to ping-pong, the transfer source is the ADC Sample
// Sequence Result FIFO 0 register, and the destination is the receive
// "B" buffer. The transfer size is set to match the size of the buffer.
//
uDMAChannelTransferSet(UDMA_CHANNEL_ADC0 | UDMA_ALT_SELECT,
UDMA_MODE_PINGPONG,
(void *)(ADC0_BASE + ADC_O_SSFIFO0),
&pui16ADCBuffer2,ADC_SAMPLE_BUF_SIZE * Channels);
//
// Set the USEBURST attribute for the uDMA ADC0 channel. This will force
// the controller to always use a burst when transferring data from the
// TX buffer to the UART. This is somewhat more efficient bus usage than
// the default which allows single or burst transfers.
//
uDMAChannelAttributeEnable(UDMA_CHANNEL_ADC0, UDMA_ATTR_USEBURST);
// Enables DMA channel so it can perform transfers. As soon as the
// channels are enabled, the peripheral will issue a transfer request and
// the data transfers will begin.
//
uDMAChannelEnable(UDMA_CHANNEL_ADC0);
}
//*****************************************************************************
//
// Configure ADC0 and use Sequencer 3 to take temperature sensor sample
//
//*****************************************************************************
void
adcConfigure()
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_2 | GPIO_PIN_3);
SysCtlDelay(80u);
// Use ADC0 sequence 0 to sample channel 0 once for each timer period
ADCClockConfigSet(ADC0_BASE, ADC_CLOCK_SRC_PLL | ADC_CLOCK_RATE_FULL, 8);
SysCtlDelay(10); // Time for the clock configuration to set
IntDisable(INT_ADC0SS0);
ADCIntDisable(ADC0_BASE, 0u);
ADCSequenceDisable(ADC0_BASE,0u);
// With sequence disabled, it is now safe to load the new configuration parameters
ADCSequenceConfigure(ADC0_BASE, 0u, ADC_TRIGGER_TIMER, 0u);
ADCSequenceStepConfigure(ADC0_BASE,0u,0u,ADC_CTL_CH0);
ADCSequenceStepConfigure(ADC0_BASE,0u,1u,ADC_CTL_CH1 | ADC_CTL_END | ADC_CTL_IE);
ADCSequenceEnable(ADC0_BASE,0u); //Once configuration is set, re-enable the sequencer
ADCIntClear(ADC0_BASE,0u);
//
// Enables the DMA channel for the ADC0 sample sequence 0.
//
ADCSequenceDMAEnable(ADC0_BASE, 0);
ADCIntEnable(ADC0_BASE, 0u);
IntEnable(INT_ADC0SS0);
}
void uartConfigure(void)
{
// Enable the peripherals used by this example.
//
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
// Set GPIO A0 and A1 as UART pins.
//
MAP_GPIOPinConfigure(GPIO_PA0_U0RX);
MAP_GPIOPinConfigure(GPIO_PA1_U0TX);
MAP_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//
// Configure the UART for 115,200, 8-N-1 operation.
//
MAP_UARTConfigSetExpClk(UART0_BASE, g_ui32SysClock, 115200,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE));
//
// Enable the UART interrupt.
//
MAP_IntEnable(INT_UART0);
MAP_UARTIntEnable(UART0_BASE, UART_INT_RX | UART_INT_RT);
}
uint32_t ui32Count;
//*****************************************************************************
//
// This example demonstrates the use of the Ethernet Controller and ADC
// peripheral.
//
//*****************************************************************************
int
main(void)
{
//
// Make sure the main oscillator is enabled because this is required by
// the PHY. The system must have a 25MHz crystal attached to the OSC
// pins. The SYSCTL_MOSC_HIGHFREQ parameter is used when the crystal
// frequency is 10MHz or higher.
//
SysCtlMOSCConfigSet(SYSCTL_MOSC_HIGHFREQ);
//
// Run from the PLL at 120 MHz.
// Note: SYSCTL_CFG_VCO_240 is a new setting provided in TivaWare 2.2.x and
// later to better reflect the actual VCO speed due to SYSCTL#22.
//
g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN |
SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_240), 120000000);
//
// Initialize the buffer status.
//
pui32BufferStatus[0] = FILLING;
pui32BufferStatus[1] = EMPTY;
//
// Configure the device pins.
//
// PinoutSet(true, false);
//
//
// Enable the GPIO port that is used for the on-board LED.
//
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
//
// Configure Port N1 for as an output for the animation LED.
//
MAP_GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_1);
//
// Initialize LED to OFF (0).
//
MAP_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, ~GPIO_PIN_1);
//
// Configure UART.
//
uartConfigure();
//
// Clear the terminal and print banner.
//
//
// Configure the ADC peripheral.
//
uDMAConfigure();
adcConfigure();
init_TIMER();
//
MAP_IntPrioritySet(INT_UART0,89);
MAP_IntPrioritySet(INT_ADC0SS0,90);
IntMasterEnable();
TimerEnable(TIMER0_BASE, TIMER_A);
// UARTSend((uint8_t *)"\033[2JEnter text: ", 16);
//
// Loop forever, processing the LED blinking. All the work is done in
// interrupt handlers.
while(1)
{
// Check if the first buffer is full, if so process data.
//
if(pui32BufferStatus[0] == FULL)
{
uint16_t j,i;
uint8_t UARTBuf[15];
//
// Process the data in pui16ADCBuffer1 and clear buffer entries.
//
for(i =0; i < ADC_SAMPLE_BUF_SIZE; i++)
{
for (j=0; j < Channels; j++ )
{
usprintf((char *)UARTBuf, "#%04X",pui16ADCBuffer1[i][j]);
UARTSend(UARTBuf, strlen((char *)UARTBuf));
UARTCharPutNonBlocking(UART0_BASE, '\n');
pui16ADCBuffer1[i][j] = 0;
}
}
pui32BufferStatus[0] = EMPTY;
//
// Enable for another uDMA block transfer.
//
uDMAChannelTransferSet(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT,
UDMA_MODE_PINGPONG,
(void *)(ADC0_BASE + ADC_O_SSFIFO0),
&pui16ADCBuffer1, ADC_SAMPLE_BUF_SIZE *Channels);
//
// Enable DMA channel so it can perform transfers.
//
uDMAChannelEnable(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT);
}
//
// Check if the second buffer is full, if so process data.
//
if(pui32BufferStatus[1] == FULL)
{
uint16_t j,i;
uint8_t UARTBuf[15];
for(i =0; i < ADC_SAMPLE_BUF_SIZE; i++)
{
for (j=0; j < Channels; j++ )
{
usprintf((char *)UARTBuf, "#%04X",pui16ADCBuffer2[i][j]);
UARTSend(UARTBuf, strlen((char *)UARTBuf));
pui16ADCBuffer2[i][j] = 0;
}
UARTCharPutNonBlocking(UART0_BASE, '\n');
}
//
// Indicate the Buffer data as been processed so new data can
// be stored.
//
pui32BufferStatus[1] = EMPTY;
//
// Enable for another uDMA block transfer.
//
uDMAChannelTransferSet(UDMA_CHANNEL_ADC0 | UDMA_ALT_SELECT,
UDMA_MODE_PINGPONG,
(void *)(ADC0_BASE + ADC_O_SSFIFO0),
&pui16ADCBuffer2, ADC_SAMPLE_BUF_SIZE *Channels);
//
// Enable DMA channel so it can perform transfers.
//
uDMAChannelEnable(UDMA_CHANNEL_ADC0 | UDMA_ALT_SELECT);
}
}
}
void init_TIMER()
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
TimerConfigure(TIMER0_BASE, TIMER_CFG_SPLIT_PAIR | TIMER_CFG_A_PERIODIC);
// Set sample frequency to 1MHz (every 1uS)
TimerLoadSet(TIMER0_BASE, TIMER_A, 65535); //TODO: Timer Load Value is set here
TimerControlTrigger(TIMER0_BASE, TIMER_A, true);
TimerControlStall(TIMER0_BASE, TIMER_A, true); //Assist in debug by stalling timer at breakpoints
}
void ADC0SS0IntHandler(void)
{
//
// Clear the Interrupt Flag.
//
ADCIntClear(ADC0_BASE, 0);
if ((uDMAChannelModeGet(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT) ==
UDMA_MODE_STOP) &&
(pui32BufferStatus[0] == FILLING))
{
pui32BufferStatus[0] = FULL;
pui32BufferStatus[1] = FILLING;
}
else if ((uDMAChannelModeGet(UDMA_CHANNEL_ADC0 | UDMA_ALT_SELECT) ==
UDMA_MODE_STOP) &&
(pui32BufferStatus[1] == FILLING))
{
pui32BufferStatus[0] = FILLING;
pui32BufferStatus[1] = FULL;
}
}