Part Number: TMDS243EVM
Hello,
I've learned that there is the must to allocate the DMA resources in early stage.
(I wanted to use 2SPIs and 7UARTs with packet DMA and it was not possible with default SBL provided):
So, I've changed the resource allocation according to https://software-dl.ti.com/mcu-plus-sdk/esd/AM243X/latest/exports/docs/api_guide_am243x/RESOURCE_ALLOCATION_GUIDE.html
I've changed the packet DMA free RX and TX channel count for MAIN_0_R5_0 and shared these with MAIN_0_R5_1 (non-secure). Afterwards, I've got an error that the ring configuration is not working (these seems not to be shared).
Then I've changed the configuration again - removed the sharing and edited the RX and TX channel count for MAIN_0_R5_1. This is working now.
But by doing this, the question rises how we can change the resource allocation later in field, if a new firmware/application update does need a different DMA resource allocation?
Is it possible to change the allocation during run-time by the application?
If this is not possible and we need to update the SBL too, how can we update the SBL in a safe way even if the power fails during update?
best regards
Bastian