Part Number: AM2634
Other Parts Discussed in Thread: BP-AM2BLDCSERVO, LP-AM263, SYSCONFIG, LP-AM243
Good day,
On the board BP-AM2BLDCSERVO SPI interface is connected as follows (using BoosterPack connector's numbers):
SPI_CLK: J5-47
SPI_CS0: J6-58
SPI_D0: J6-55
SPI_D1: J6-54
On the LP-AM263 board, they are mapped as follows:
J5-47: SPI1_CLK
J6-58: SPI1_Cs0
J6-55: SPI0_D0
J6-54: SPI0_D1
The problem is that I cannot configure an SPI controller so it uses these pins. Sysconfig allows to configure all pins from SPI0 or all pins from SPI1, but does not allow to mix them. Please advise how should I configure the SPI to work with these boards.
Regards,
Dmitry