Part Number: SAFETI_DIAG_LIB
Other Parts Discussed in Thread: RM48L540
Hi,
I am using RM48Lx40 series controller and I have integrate RM48x50 SafeTi library in my application but I have to modified command in file but still code is not working. Please check both and let me know if any update.
SafeTi sys_link.cmd file
/* Memory Map */
MEMORY
{
VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH0 (RX) : origin=0x00000020 length=0x0017FFE0
FLASH1 (RX) : origin=0x00180000 length=0x00180000
STACKS (RW) : origin=0x08000000 length=0x00001800
RAM (RW) : origin=0x08008000 length=0x00028000
PROFILE(RW) : origin=0x08036000 length=0x00008000 /* Added for profiling purposes */
LOG (RW) : origin=0x080053B0 length=0x00002000 fill=0xDEADBEEF/* Added for logging purposes */
FEE (R) : origin=0xF0200000 length=0x00000064 fill=0xDEADBEEF /* For FEE testing, Valid only for sample application */
}
My application RM48l540 updated memory map
#if 0
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Memory Map */
MEMORY
{
VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH0 (RX) : origin=0x00000020 length=0x0017FFE0
FLASH1 (RX) : origin=0x00180000 length=0x00080000
STACKS (RW) : origin=0x08000000 length=0x00001500
RAM (RW) : origin=0x08001500 length=0x0002EB00
/* USER CODE BEGIN (2) */
/* USER CODE END */
}
/* USER CODE BEGIN (3) */
#endif
/*----------------------------------------------------------------------------*/
/* Memory Map */
MEMORY
{
VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH0 (RX) : origin=0x00000020 length=0x0017FFE0
FLASH1 (RX) : origin=0x00180000 length=0x00080000
STACKS (RW) : origin=0x08000000 length=0x00001800
RAM (RW) : origin=0x08001800 length=0x00021800
PROFILE(RW) : origin=0x08036000 length=0x00008000 /* Added for profiling purposes */
LOG (RW) : origin=0x08023000 length=0x00002000 fill=0xDEADBEEF/* Added for logging purposes */
FEE (R) : origin=0xF0200000 length=0x00000064 fill=0xDEADBEEF /* For FEE testing, Valid only for sample application */
}