Part Number: AM2634
When I look at the AM263x documentation, it seems that it is not possible to configure outputs in an open-drain mode.
Is this true?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM2634
When I look at the AM263x documentation, it seems that it is not possible to configure outputs in an open-drain mode.
Is this true?
Hello,
There is not an official "Open-drain mode" for the general LVCMOS voltage buffers which are used for a majority of the pins on the device. However, if you select one of these pins for your GPIO, they can be configured to operate as open-drain outputs by configuring the GPIO module to source a constant low output and toggle the output enable. The output buffer will drive low when enabled and will be high impedance when disabled.
Best Regards,
Zackary Fleenor