Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: SDK contents does not show in Sysconfig completely

Part Number: AM2434
Other Parts Discussed in Thread: SYSCONFIG, TIDEP-01032

Good day,

I am trying to complete a system design for BLDC motor control with EtherCAT interface. For that I have installed MCU+SDK, INDUSTRIAL-COMMs SDK, and MOTOR-CONTROL SDK. The first problem is that in Sysconfig I see only the small part of these kits. For example, MOTOR-CONTROL SDK consists of three parts: current-sense, position-sense, and dcl. But in the Sysconfig I see only EnDat, HDSL, and Tamagawa, i.e. position-sense only. Also I see no industrial communications protocols despite it presents in the file structure (C:\ti\motor_control_sdk_am243x_09_00_00_05\ind_comms_sdk\source\industrial_comms). And when I choose INDUSTRIAL-CONTROL in Sysconfig I see only EtherCAT, Ethernet/IP, HSR-PRP and Profinet despite in the file structure there is also IOLINK. Please advise how could I bring all these kits to work together. 

Regards,

Dmitry