Other Parts Discussed in Thread: AM69
Dear Support,
The data sheets indicate in each case:
- AM62x: 315MPixel/s, 1x CSI-2 4L
- AM68x: 480MPixel/s, 2x CSI-2 4L
- AM69x: 2x480MPixel/s, 3x CSI-2 4L
1. AM62x: If I want to connect 2 cameras here, I saw that a bridge can be used. Is the ISP then divided equally? (157MPixel/s per camera)?
2. AM68x: There are already two camera interfaces here. Is the ISP split when using both interfaces? If so, half and half?
3. AM69x: 2x VPAC and 3x interface are specified here. How is the ISP divided here if 2 or 3 cameras are connected?
Many thanks for your support!
regards
Stefan