Part Number: MCU-PLUS-SDK-AM243X
HI team,
We are using the "profinet rt rgmii demo example in MCU-PLUS-SDK-AM243X Version 08_06_00_48", and it works perfectly. but when we change ObjectUUID_LocalIndex="1" to ObjectUUID_LocalIndex="0," then the profinet device is not connecting to the master.
If we want to connect a profinet device to a master, what do we need to do in profinet device?