Part Number: MSPM0G3507
Other Parts Discussed in Thread: MSPM0L1306
Looking for an example of how to change pin use temporarily at runtime. EG: when a pin was originally configured as a Output Pin but need to flip back and forth between input and output at runtime for a RC circuit. I can do this with most other CPU and other SDK but could not find documentation on how to do it with the MSPM0 without RTOS.
In this application I need first to convert the and OUTPUT and drive it LOW to discharge a variable capacitor. Then I want to convert it back to input feeding the OP AMP - (inverting input) to record how long it takes charge the capacitor. I can do it with a external pchannel mosfet but this is easy for both the ATMEL Tiny CPU running bascom and the ESP32 running Arduino.
I need this to work on both a MSPM0L1306 and MSPM0G3507.
I would also love a example of changing the PIN MUX config at runtime so I could switch to different input pins to feed the OpAmp1 - inverting input.
These examples would be best if shown how to accomplish this without the RTOS.