Part Number: AM2631
Hello,
For my project it is necessary to achieve the following frequencies to interface with peripherals:
GPCM: 21.33 MHZ (64 MHz/3)
CLKOUT0: 64 MHz
CLKOUT1: 21.33 MHZ (64 MHz/3)
(besides, periodic interrupts of 2ms and 22ms are also required)
Is it necessary to modify the Core/Peripheral/SYS_CLK frequencies, or can they be achieved just by modifying the peripherals' frequency dividers? The suggested external clock of 25MHz is populated and the root clocks (as in Table 6-25 Root clocks table) used for the time being.
Regards,
Javier