Part Number: EK-TM4C1294XL
Other Parts Discussed in Thread: ENERGIA, TM4C1294NCPDT
I'm starting a project with EK-TM4C1294XL, using ENERGIA IDE, I have flashed a test code sending SPI messages, and I can see the SPI frames(so code is running), but now I can't re flash due an error connecting to the target.
I'm afraid I use an incorrect port (26) for the SPI SS (CS), and may be it is affecting the connection with the target:

Is there any way to force the re-flashing? Any way to erase the code? Or any way to recover the communication?
Thank's in advance!
Fran