Hİ,
I'am using tms570. I programmed it to send CAN meesages constantly boud rate at 250kbit. I listen CAN messages via peak view. I set baudrate at 250kbit at peak view too. But if I set Peak view boud rate higher at first such as 1Mbit and then to 250kbit, it stops sending CAN messages until I power-off and on to chip. IF I set peak view bod rate to 5 kbit and then to 250kbit it keeps sending the CAN messages, doesn't require to power off and on. Only if I set it higher at first. What it can be the cause of it ?
Thank you.