This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-MSPM0G3507: CAN interface

Part Number: LP-MSPM0G3507


Hello TI,,

I am recently  go through the LP-MSPM0G3507 for CAN -FD interface , I get some example code for the same on  the Resource explore , so I simply took the example code and modify  the same in order to transmat the data continuously without any other function and as per my understanding as I flash the code inside the MCU it should give some signal on Tx pin of CAN , I connect the Tx Pin ( as I know CAN Tx and Rx pin was PA12  and PA13)

of CAN to Oscilloscope with respect to GND to check the Tx pin signal , as I flash the code I always getting HIGH signal (I expect that should be high low kind of thing there is that not ? ), Please let me know how i can check the CAN module with help of Oscilloscope or less peripheral.

Thanks and regards,

Karan Rajput