Part Number: LP-MSPM0G3507
Other Parts Discussed in Thread: MSPM0G3507
Hello TI,,
I am recently go through the LP-MSPM0G3507 for CAN -FD interface , I get some example code for the same on the Resource explore , so I simply took the example code and modify the same in order to transmat the data continuously without any other function and as per my understanding as I flash the code inside the MCU it should give some signal on Tx pin of CAN , I connect the Tx Pin ( as I know CAN Tx and Rx pin was PA12 and PA13)
of CAN to Oscilloscope with respect to GND to check the Tx pin signal , as I flash the code I always getting HIGH signal (I expect that should be high low kind of thing there is that not ? ), Please let me know how i can check the CAN module with help of Oscilloscope or less peripheral.
Thanks and regards,