Part Number: TMS570LC4357-EP
Other Parts Discussed in Thread: HALCOGEN, TMS570LC4357
Hello:
How to set the offset address of the interrupt vector table based on TMS570 platform?
Thank you!
Jiangbo Hu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LC4357-EP
Other Parts Discussed in Thread: HALCOGEN, TMS570LC4357
Hello:
How to set the offset address of the interrupt vector table based on TMS570 platform?
Thank you!
Jiangbo Hu
Hi Jiangbo,
Do you mean offset address in VIM table? Please refer to interrupt request assignments (table 6-39) in device datasheet (SPNS195C).
In the HalCoGen generated code, the interrupt table is s_vim_init[..]:
static const t_isrFuncPTR s_vim_init[128U] =

I means:

As shown in the figure, it is in the cmd file.
If I want to put the VECTORS to the start address that 0x60000000, I modified the origin = 0x60000000.
Do I need to make any other settings except that "modified the origin = 0x60000000"?
No, TMS570 doesn't have ROM bootloader, and supports only bootloader in the flash.
No, TMS570 doesn't have ROM bootloader, and supports only bootloader in the flash.
Thank you!
Is there any documentation or datasheet explaining this viewpoint?
Page 1 of the device datasheet:

The device doesn't have a boot ROM. After reset (warm-reset or power on reset) is released, the CPU fetches the first instruction from address
0x00000000
The flash libraries for TMS570LC4357 are:
1. F021_API_CortexR4_BE_L2FMC_V3D16_NDS.lib: This is the Flash API object file without debug symbols for Cortex R4/R5 Big Endian devices using the L2FMC memory controller and floating point unit.
2. F021_API_CortexR4_BE_L2FMC_V3D16.lib: This is the Flash API object file for Cortex R4/R5 Big Endian devices using the L2FMC memory controller and floating point unit.
3. F021_API_CortexR4_BE_L2FMC_NDS.lib: This is the Flash API object file without debug symbols for Cortex R4 Big Endian devices using the L2FMC memory controller
4. F021_API_CortexR4_BE_L2FMC.lib: This is the Flash API object file for Cortex R4 Big Endian devices using the L2FMC memory controller.
You can use our bootloader (CAN, SPI, Ethernet, UART) as examples. The bootloader use Flash API to erase flash sectors and program data to flash.
1452.TMS570LC4357_UART_BootLoader.zip
/*****************************************************************************
*
* bl_flash.c : The file holds the main control loop of the boot loader.
* Author : QJ Wang. qjwang@ti.com
* Date : 4-19-2019
*/
/* Copyright (C) 2013-2019 Texas Instruments Incorporated - http://www.ti.com/
*
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
//*****************************************************************************
#include "bl_config.h"
#include "bl_flash.h"
#include "F021.h"
#include "flash_defines.h"
//#define Freq_In_MHz = SYS_CLK_FREQ;
uint8_t g_ucStartBank, g_ucEndBank, g_ucStartSector, g_ucEndSector;
uint32_t g_ulBankInitialized = 0;
//*****************************************************************************
//
// Returns the size of the ist sector size of the flash in bytes.
//
//*****************************************************************************
uint32_t
BLInternalFlashFirstSectorSizeGet(void)
{
uint32_t firstSectorSize;
firstSectorSize = (uint32_t)(flash_sector[0].start) + flash_sector[0].length;
return (firstSectorSize);
}
//*****************************************************************************
//
// Returns the size of the internal flash in bytes.
//
// This function returns the total number of bytes of internal flash in the
// current part. No adjustment is made for any sections reserved via
// options defined in bl_config.h.
//
// \return Returns the total number of bytes of internal flash.
//
//*****************************************************************************
uint32_t
BLInternalFlashSizeGet(void)
{
uint32_t flashSize;
flashSize = (uint32_t)flash_sector[NUMBEROFSECTORS-1].start + flash_sector[NUMBEROFSECTORS-1].length;
return (flashSize);
}
//*****************************************************************************
//
// Checks whether a given start address is valid for a download.
//
// This function checks to determine whether the given address is a valid
// download image start address given the options defined in bl_config.h.
//
// \return Returns non-zero if the address is valid or 0 otherwise.
//
//*****************************************************************************
uint32_t
BLInternalFlashStartAddrCheck(uint32_t ulAddr, uint32_t ulImgSize)
{
uint32_t count=0, i;
uint32_t ulWholeFlashSize;
//
// Determine the size of the flash available on the part in use.
//
ulWholeFlashSize = (uint32_t)flash_sector[NUMBEROFSECTORS-1].start + flash_sector[NUMBEROFSECTORS-1].length;
/* The start address must be at the beginning of the sector */
for (i = 0; i < NUMBEROFSECTORS; i++){
if ((ulAddr >= (uint32_t)(flash_sector[i].start)) && (ulAddr < ((uint32_t)flash_sector[i].start + flash_sector[i].length)))
{
count++;
}
}
if (count == 0){
return(0);
}
//
// Is the address we were passed a valid start address? We allow:
//
// 1. Address 0 if configured to update the boot loader.
// 2. The start of the reserved block if parameter space is reserved (to
// allow a download of the parameter block contents).
// 3. The application start address specified in bl_config.h.
//
// The function fails if the address is not one of these, if the image
// size is larger than the available space or if the address is not word
// aligned.
//
if((
#ifdef ENABLE_BL_UPDATE
(ulAddr != 0) &&
#endif
(ulAddr != APP_START_ADDRESS)) ||
((ulAddr + ulImgSize) > ulWholeFlashSize) ||
((ulAddr & 3) != 0))
{
return(0);
}
else {
return(1);
}
}
/* Initialize the flash bank and activate the sectors */
uint32_t Fapi_Init(uint32_t ucStartBank, uint32_t ucEndBank)
{
uint32_t i;
/*SYS_CLK_FREQ is defined in bl_config.h */
if ((Fapi_initializeFlashBanks((uint32_t)SYS_CLK_FREQ)) == Fapi_Status_Success){
for (i = ucStartBank; i < ( ucEndBank + 1); i++){
(void)Fapi_setActiveFlashBank((Fapi_FlashBankType)i);
(void)Fapi_enableMainBankSectors(0xFFFF); /* used for API 2.01*/
while( FAPI_CHECK_FSM_READY_BUSY != Fapi_Status_FsmReady );
while( FAPI_GET_FSM_STATUS != Fapi_Status_Success ); /* don't have to include this one*/
}
g_ulBankInitialized = 1;
}else {
return (1);
}
return (0); //success
}
/* ulAddr must be starting address of one flash sector*/
uint32_t Fapi_BlockErase(uint32_t ulAddr, uint32_t Size)
{
uint8_t i=0, ucStartSector, ucEndSector;
uint32_t EndAddr, status;
EndAddr = ulAddr + Size;
for (i = 0; i < NUMBEROFSECTORS; i++){
if (ulAddr < (uint32_t)(flash_sector[i].start))
{
g_ucStartBank = flash_sector[i-1].bankNumber;
ucStartSector = i-1;
break;
}
}
for (i = ucStartSector; i < NUMBEROFSECTORS; i++){
if (EndAddr <= (((uint32_t)flash_sector[i].start) + flash_sector[i].length))
{
g_ucEndBank = flash_sector[i].bankNumber;
ucEndSector = i;
break;
}
}
status = Fapi_Init(g_ucStartBank, g_ucEndBank);
for (i=ucStartSector; i<(ucEndSector+1); i++){
Fapi_issueAsyncCommandWithAddress(Fapi_EraseSector, flash_sector[i].start);
while( FAPI_CHECK_FSM_READY_BUSY == Fapi_Status_FsmBusy );
while(FAPI_GET_FSM_STATUS != Fapi_Status_Success);
}
#if defined (RM57) || defined (TMS570LC43)
status = 0;
#else
status = Flash_Erase_Check((uint32_t)ulAddr, Size);
#endif
return (status);
}
//Bank here is not used. We calculate the bank in the function based on the Flash-Start-addr
uint32_t Fapi_BlockProgram(uint32_t Flash_Address, uint32_t Data_Address, uint32_t SizeInBytes)
{
register uint32_t src = Data_Address;
register uint32_t dst = Flash_Address;
uint32_t bytes;
if (SizeInBytes < 16)
bytes = SizeInBytes;
else
bytes = 16;
/* The flash bank has been initialized in flash erase function */
if (g_ulBankInitialized |= 1 ){
Fapi_Init(g_ucStartBank, g_ucEndBank);
}
while( SizeInBytes > 0)
{
Fapi_issueProgrammingCommand((uint32_t *)dst,
(uint8_t *)src,
(uint32_t) bytes,
0,
0,
Fapi_AutoEccGeneration);
while( FAPI_CHECK_FSM_READY_BUSY == Fapi_Status_FsmBusy );
while(FAPI_GET_FSM_STATUS != Fapi_Status_Success);
src += bytes;
dst += bytes;
SizeInBytes -= bytes;
if ( SizeInBytes < 32){
bytes = SizeInBytes;
}
}
return (0);
}
uint32_t Fapi_UpdateStatusProgram(uint32_t Flash_Start_Address, uint32_t Data_Start_Address, uint32_t Size_In_Bytes)
{
register uint32_t src = Data_Start_Address;
register uint32_t dst = Flash_Start_Address;
unsigned int bytes;
if (Size_In_Bytes < 16)
bytes = Size_In_Bytes;
else
bytes = 16;
Fapi_issueProgrammingCommand((uint32_t *)dst,
(uint8_t *)src,
(uint32_t) bytes,
0,
0,
Fapi_AutoEccGeneration);
while( Fapi_checkFsmForReady() == Fapi_Status_FsmBusy );
while(FAPI_GET_FSM_STATUS != Fapi_Status_Success);
return (0);
}
uint32_t Flash_Program_Check(uint32_t Program_Start_Address, uint32_t Source_Start_Address, uint32_t No_Of_Bytes)
{
register uint32_t *src1 = (uint32_t *) Source_Start_Address;
register uint32_t *dst1 = (uint32_t *) Program_Start_Address;
register uint32_t bytes = No_Of_Bytes;
while(bytes > 0)
{
if(*dst1++ != *src1++)
return (1); //error
bytes -= 0x4;
}
return(0);
}
uint32_t Flash_Erase_Check(uint32_t Start_Address, uint32_t Bytes)
{
uint32_t error=0;
register uint32_t *dst1 = (uint32_t *) Start_Address;
register uint32_t bytes = Bytes;
while(bytes > 0)
{
if(*dst1++ != 0xFFFFFFFF){
error = 2;
}
bytes -= 0x4;
}
return(error);
}
uint32_t Fapi_BlockRead( uint32_t Flash_Start_Address, uint32_t Data_Start_Address, uint32_t Size_In_Bytes)
{
register uint32_t src = Data_Start_Address;
register uint32_t dst = Flash_Start_Address;
register uint32_t bytes_remain = Size_In_Bytes;
int bytes;
if (Size_In_Bytes < 16)
bytes = Size_In_Bytes;
else
bytes = 16;
while( bytes_remain > 0)
{
Fapi_doMarginReadByByte((uint8_t *)src,
(uint8_t *)dst,
(uint32_t) bytes, //16
Fapi_NormalRead);
src += bytes;
dst += bytes;
bytes_remain -= bytes;
}
return (0);
}