Part Number: MSP430FR2476
About MSP430FR2476
Set the internal clock to 4MHz,
I would like to use an external clock for the timer "TA0" and operate it at 40kHz.
What settings should I make in this case?
I would appreciate it if you could write the program code for setting the internal clock to 4MHz and the program code for operating "TA0" with an external clock.
Thank you.