This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: MSPM0G3507 LaunchPad Development Kit

Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG

hello team 

My question related to MCAN .  My setup is decribed below .

1) I have a my own MCPM0G3507  board  with external can ic is using for transmitting and receiving the data. 

2) when I am using MCAN RX sample code in that . it is working fine . in my  code also initilize a GPIO and connected to LED , am sending a data and and checking LED is glowing or not . it is working fine .

3) for transmitting or receiving the data an using Kvaser can communication module  ( 500 kb/s ).

4)  In same  receiving  code I want to add transmitting data  . i checked tx sample code they are using gpio interrupt . but  my code i am not using  any goio interrupt , my code is - if rx data is coming then i have to send tx data to my analyzer .  same setting i done in my code like as sample code ( except gpio interrupt) .  i am using only one interrupt for receiving a data . after receiving have to send to tx data to analyser . will it work or not .

5) for transmitting a data interrupt is compulsory . if not why is not working if i am combining RX  and TX both at a  time . Rx is working properly . 

6) if you have any sample code both tx and rx combine working properly please suggest me . 

This is urgent for me . please help me 

thanks and regards 

Aryan vats