Part Number: TMS570LS3137

Base on this DS, the max power = 235-0.15*exp(0.174Tjk). I don't see how the power can be higher than 235 ma from this equation. In addition, the power will be less at higher temperature. Please explain.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LS3137

Base on this DS, the max power = 235-0.15*exp(0.174Tjk). I don't see how the power can be higher than 235 ma from this equation. In addition, the power will be less at higher temperature. Please explain.
Hi Tam,
Please have a look at below similar issue that we got recently and this might be useful for you:
--
Thanks & regards,
Jagadish.
Thanks for sending the .pdf. However, there is no answer to my question. In fact the other person had the same question. I don't see how you get 700 mA max current and even at 25C the equation did not come out as in the datasheet.
The maximum ICC with HCLK=180MHz at 150degree junction-temperature during LBIST is 700mA.
If junction temperature is 25 degree, the Icc = 700 -{ 235 - 0.15e(0.0174*298.15)} = 700 - 57.67 = 642.3 mA
If junction temperature is 150 degree, the Icc = 700 -{ 235 - 0.15e(0.0174*423.15)} = 700 - 0.012 = 699.99 mA
The formula (235 - 0.15*e0.0174TJK) is for derating or subtraction from the maximum current.