Part Number: TMS570LC4357
Hello,
I have a question regarding the MPU configuration.
What happens if two MPU regions have the same Region Base Address but different settings for the address area.
Which configuration will the CPU use.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LC4357
Hello,
I have a question regarding the MPU configuration.
What happens if two MPU regions have the same Region Base Address but different settings for the address area.
Which configuration will the CPU use.
Thanks
Hi David,
Please look into below FAQ:

When memory regions overlap, memory access is affected by the attributes of the region with the highest number.
For example, if memory regions 3 and 4 regions have same base address with different MPU settings then the corresponding memory region will be affected by the region-4 settings.
--
Thanks & regards,
Jagadish.