Part Number: AM2431
Is there any problem if the pin is HIZ when "The input buffer is disabled.
If the CMOS input is HIZ, a through-current may flow, resulting in a failure.
When "The input buffer is disabled." is it safe to assume that the pin is in a state where measures have been taken to prevent through-current flow?
<Background explanation
I use the pin as a GPIO output.
After reset, the pin is HIZ until the GPIO_DIR** register is set to output.
At this time, I am concerned about through-current flow to the CMOS input stage.