Part Number: TM4C129ENCPDT
Hi,
I have configured the Internal ADC of the microcontroller. I am receiving correct values for AIN0, AIN1, AIN2, AIN3, however for AIN8 and AIN9 it would be spitting wrong values. I am guessing, if it has something to do with the order of the channels since there is missing ADC channels between AIN3 and AIN8.
I have configured Port E of the controller for the above signals.
Here is my code;
The port pin definitions are below;
uint32_t IntADCRawData0[8]; //Buffer array that holds ADC samples
//On Board ADC Signals Pins map connected to microcontroller internal ADC
#define ADC_PIN_33Volt GPIO_PIN_0
#define ADC_PIN_5Volt GPIO_PIN_1
#define ADC_PIN_15NegVolt GPIO_PIN_2
#define ADC_PIN_15PosVolt GPIO_PIN_3
#define ADC_PIN_VCF GPIO_PIN_4
#define ADC_PIN_VC2 GPIO_PIN_5
#define ADC_CH_33Volt ADC_CTL_CH3 //PE0 = AIN3
#define ADC_CH_5Volt ADC_CTL_CH2 //PE1 = AIN2
#define ADC_CH_15NegVolt ADC_CTL_CH1 //PE2 = AIN1
#define ADC_CH_15PosVolt ADC_CTL_CH0 //PE3 = AIN0
#define ADC_CH_VCFVolt ADC_CTL_CH9 //PE4 = AIN9
#define ADC_CH_VC2Volt ADC_CTL_CH8 //PE5 = AIN8
The ADC init function is here;
void Internal_ADC0_Init(void)
{
//First configure common ADC Ports and Pins
// *** Peripheral Enable
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
ROM_SysCtlPeripheralReset(SYSCTL_PERIPH_GPIOE);
SysCtlDelay(100);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
SysCtlDelay(100);
//Configure the individual pins being used as ADC input pins
ROM_GPIOPinTypeADC(GPIO_PORTE_BASE, ADC_PIN_VC2 | ADC_PIN_VCF | ADC_PIN_15PosVolt | ADC_PIN_15NegVolt | ADC_PIN_5Volt | ADC_PIN_33Volt);
ROM_ADCReferenceSet(ADC0_BASE,ADC_REF_INT);
ROM_ADCSequenceDisable(ADC0_BASE, 0); //Disable sequence before we change it
ROM_ADCSequenceConfigure(ADC0_BASE,0,ADC_TRIGGER_PROCESSOR,0); //ADC Trigger by Processor
ROM_ADCSequenceStepConfigure(ADC0_BASE,0,0,ADC_CH_15PosVolt); //To sample Channel 0
ROM_ADCSequenceStepConfigure(ADC0_BASE,0,1,ADC_CH_15NegVolt); //To sample Channel 1
ROM_ADCSequenceStepConfigure(ADC0_BASE,0,2,ADC_CH_5Volt); //To sample Channel 2
ROM_ADCSequenceStepConfigure(ADC0_BASE,0,3,ADC_CH_33Volt); //To sample Channel 3
ROM_ADCSequenceStepConfigure(ADC0_BASE,0,4,ADC_CH_VC2Volt); //To sample Channel 8
ROM_ADCSequenceStepConfigure(ADC0_BASE,0,5,ADC_CH_VCFVolt); //To sample Channel 9
ROM_ADCHardwareOversampleConfigure(ADC0_BASE, 64); //Configure the hardware Averager module to average out 64 samples for each channel.
ROM_ADCSequenceStepConfigure(ADC0_BASE,0,6,ADC_CTL_TS|ADC_CTL_IE|ADC_CTL_END);
ROM_ADCSequenceEnable(ADC0_BASE,0);
}
After initialization, I call the following function to collect data and save in different variables.
//This function collects data from internal ADC and saves at the pointer location.
void IntADC_Collect_Data(void)
{
// Trigger the sample sequence.
ADCProcessorTrigger(ADC0_BASE, 0);
//while(!ADCIntStatus(ADC0_BASE, 0, false)){} //DO NOT use this while loop as it may take forever instead use a delay
vTaskDelay(10/portTICK_PERIOD_MS); // 10msec delay
ADCSequenceDataGet(ADC0_BASE, 0, IntADCRawData0);
volt15Pos.data.value16bits = 0x0000FFFF & IntADCRawData0[0];
volt15Neg.data.value16bits = 0x0000FFFF & IntADCRawData0[1];
volt5.data.value16bits = 0x0000FFFF & IntADCRawData0[2];
volt33.data.value16bits = 0x0000FFFF & IntADCRawData0[3];
VC2DAC_ReadBack.data.value16bits = 0x0000FFFF & IntADCRawData0[4];
VCFDAC_ReadBack.data.value16bits = 0x0000FFFF & IntADCRawData0[5];
ProcessorTemp.data.value16bits = 0x0000FFFF & IntADCRawData0[6];
Kicker_Spare_Temp.data.value16bits = 0x0000FFFF & IntADCRawData0[7]; //This is just a place holder since in case of Septum Kicker_Spare_Temp doesnt exist
}
As I said earlier, We can read correctly all values for AIN0, AIN1, AIN2, AIN3, however for AIN8 and AIN9 are not reporting correct values.
Any idea / hint ?
Thanks