Part Number: TM4C129ENCPDT
Hello Charles,
I hope you doing well.
I am facing another weird issue. I have two interrupts on GPIO_PORTM_BASE one is at GPIO_PIN_3 i.e. PM3 another is GPIO_PIN_6 i.e. PM6. GPIO_PIN_6 interrupt will always get triggered and land the cpu into the interrupt handler routine while GPIO_PIN_3 interrupt triggers the CPU into the interrupt handler routine for first few cycles. However after some time later, the CPU will not get triggered from GPIO_PIN_3 anymore, I scoped the interrupt signal on GPIO_PIN_3 and I can see the interrupt signal is always there as expected.
GPIO_PIN_3 is a periodic interrupt running at 15msec while GPIO_PIN_6 is a push button that you triggers the ISR whenever user push the button.
GPIO_PIN_6 will always trigger CPU.
Here is my code.
The defines are;
#define PSONOFFRESET_RQST_PORT GPIO_PORTM_BASE #define PSONOFFRESET_RQST_PIN GPIO_PIN_6 //PM6 #define ADC_CTRL_PORT GPIO_PORTM_BASE #define ADC_BUSY GPIO_PIN_3 //PM3
The ISR is here;
//Interrupt Service Routine
void PORTM_Common_IntHandler(void)
{
// Clear the interrupt
uint32_t status;
SysCtlDelay(10);
status = GPIOIntStatus(ADC_CTRL_PORT, true);
if(status & ADC_BUSY)
{
ExtADC_Collect_Data();
}
else if (status & PSONOFFRESET_RQST_PIN)
{
Global_Flag = 1;
}
}
GPIOIntClear(ADC_CTRL_PORT, status);
}
//Enable GPIO_PIN_6 interrupt function
void PS_ONOFFRESET_Req_interrupt_enable(void)
{
IntMasterDisable();
GPIOPinTypeGPIOInput(PSONOFFRESET_RQST_PORT, PSONOFFRESET_RQST_PIN);
GPIOPadConfigSet(PSONOFFRESET_RQST_PORT, PSONOFFRESET_RQST_PIN, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPU); // Enable weak pullup resistor for ADC_BUSY
GPIOIntDisable(PSONOFFRESET_RQST_PORT, PSONOFFRESET_RQST_PIN);
GPIOIntClear(PSONOFFRESET_RQST_PORT, PSONOFFRESET_RQST_PIN);
GPIOIntRegister(PSONOFFRESET_RQST_PORT, PORTM_Common_IntHandler);
GPIOIntTypeSet(PSONOFFRESET_RQST_PORT, PSONOFFRESET_RQST_PIN, GPIO_LOW_LEVEL);
GPIOIntEnable(PSONOFFRESET_RQST_PORT, PSONOFFRESET_RQST_PIN);
IntMasterEnable();
}
//Enable GPIO_PIN_3 interrupt function
void ExtADC_Busy_interrupt_enable(void)
{
//Enable Interrupt on ADC_BUSY Pin
IntMasterDisable();
GPIOPinTypeGPIOInput(ADC_CTRL_PORT, ADC_BUSY);
GPIOPadConfigSet(ADC_CTRL_PORT, ADC_BUSY, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPD);
GPIOIntDisable(ADC_CTRL_PORT, ADC_BUSY);
GPIOIntClear(ADC_CTRL_PORT, ADC_BUSY);
GPIOIntRegister(ADC_CTRL_PORT, PORTM_Common_IntHandler);
GPIOIntTypeSet(ADC_CTRL_PORT, ADC_BUSY, GPIO_FALLING_EDGE);
GPIOIntEnable(ADC_CTRL_PORT, ADC_BUSY);
IntMasterEnable();
}
Not sure, what is going wrong.
Thanks for help.
Regards