Part Number: MSP432E401Y
Hi,
How can I detect link-layer events, specifically link-up/down events? We are using the simplelink_msp432e4_sdk_4_20_00_12.
Regards,
-Mike
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432E401Y
Hi,
How can I detect link-layer events, specifically link-up/down events? We are using the simplelink_msp432e4_sdk_4_20_00_12.
Regards,
-Mike
Hi Mike,
Please refer to the EMACMSP432E4_processPhyInterrupt function. You can use this function to detect the link status. This function is in C:\ti\simplelink_msp432e4_sdk_4_20_00_12\source\ti\drivers\emac\EMACMSP432E4.c.
/*
* ======== EMACMSP432E4_processPhyInterrupt ========
*/
static void EMACMSP432E4_processPhyInterrupt()
{
uint16_t value;
uint16_t status;
uint32_t config;
uint32_t mode;
uint32_t rxMaxFrameSize;
/*
* Read the PHY interrupt status. This clears all interrupt sources.
* Note that we are only enabling sources in EPHY_MISR1 so we don't
* read EPHY_MISR2.
*/
value = EMACPHYRead(EMAC0_BASE, PHY_PHYS_ADDR, EPHY_MISR1);
/* Read the current PHY status. */
status = EMACPHYRead(EMAC0_BASE, PHY_PHYS_ADDR, EPHY_STS);
/* Has the link status changed? */
if (value & EPHY_MISR1_LINKSTAT) {
/* Is link up or down now? */
if (status & EPHY_STS_LINK) {
EMACMSP432E4_private.linkUp = true;
}
else {
EMACMSP432E4_private.linkUp = false;
}
/* Signal the stack for this link status change (from ISR) */
signalLinkChange(EMACMSP432E4_private.hEvent,
EMACMSP432E4_private.linkUp, 1);
}
/* Has the speed or duplex status changed? */
if (value & (EPHY_MISR1_SPEED | EPHY_MISR1_DUPLEXM | EPHY_MISR1_ANC)) {
/* Get the current MAC configuration. */
EMACConfigGet(EMAC0_BASE, (uint32_t *)&config, (uint32_t *)&mode,
(uint32_t *)&rxMaxFrameSize);
/* What speed is the interface running at now? */
if (status & EPHY_STS_SPEED) {
/* 10Mbps is selected */
config &= ~EMAC_CONFIG_100MBPS;
}
else {
/* 100Mbps is selected */
config |= EMAC_CONFIG_100MBPS;
}
/* Are we in full- or half-duplex mode? */
if (status & EPHY_STS_DUPLEX) {
/* Full duplex. */
config |= EMAC_CONFIG_FULL_DUPLEX;
}
else {
/* Half duplex. */
config &= ~EMAC_CONFIG_FULL_DUPLEX;
}
/* Reconfigure the MAC */
EMACConfigSet(EMAC0_BASE, config, mode, rxMaxFrameSize);
}
}Hi Mike,
Looking through the PHY registers, I don't really any registers collecting errors at the Ethernet connection level other than the EPHYSTAT register which is being read by EMACMSP432E4_processPhyInterrupt. What specific errors are you looking for?
/* Read the current PHY status. */
status = EMACPHYRead(EMAC0_BASE, PHY_PHYS_ADDR, EPHY_STS);