This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS1114: performance and code analysis

Part Number: TMS570LS1114

Hello,

We have an existing code, which cause a reset of the controller in rare cases. The investigation so far has not been able to further narrow down the circumstances of the reset.

We can use TRACE32 Performance Analyzer over JTAG, but it works only with the "PERF.METHOD StopAndGo". Typically, the view shows only around 80% runtime.

The communication interfaces are already in use and do not provide enough capacity to send further messages. It is also an additional code, which leads to a performance issue with the timing.

Is there an option to trace or analyze the code execution without intrusion?

Which further options are possible to analyze and get performance information about an existing code?

thanks,

regards,