Part Number: MCU-PLUS-SDK-AM243X
Hello,
I am looking at the documentation for the usage of the SA2UL APIs for SHA hashing, as well as the examples in the SDK, and I am not sure of the correct usage. In the documentation here:
AM243x MCU+ SDK: SA2UL (ti.com)
The output buffer given to SA2UL_contextProcess is the size of the resulting hash (e.g. 512 bits or 64 bytes). However in the examples provided in the SDK (e.g. examples\security\crypto\sa2ul_sha\crypto_sha.c), the output buffer is the same size as the input buffer, and the resulting hash is found in gSa2ulCtxObj.computedHash. Which is the intended behavior?
Is it really necessary to include a buffer of the same size as the input even if it's not used when computing the SHA hash? Currently this is the only way I am able to get it to work, but it is wasteful when computing the hash of a large buffer as I have to allocate twice the space for it.
Thank you