Part Number: MSPM0L1306
Other Parts Discussed in Thread: TMDSEMU110-U,
I would like to connect the PC and MSPM0L1306 using TMDSEMU110-U.
"Error connecting to the target:
DAP Connection Error. This could be caused by the device having gone to low power mode.
Try forcing an external reset.If the error persists, try forcing BSL, a Mass erase or a Factory Reset. Check device FAQs for more information.
An error will appear.
Could it be that the circuit is bad or the timing of the power supply and reset is wrong?
Or is the TMDSEMU110-U connected incorrectly?
Create the circuit and make the first connection.
I did an external reset, but the same error occurs.