Other Parts Discussed in Thread: CC1354P10, , LP-XDS110ET
CC1354P10 EVK hardware more than 2 EVK boards in same PC it is getting detected in UNIFLASH software but when we try to flash the program we are getting the below error message in UNIFLASH tool
Error initializing emulator: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the XDS110SupportReadMe.pdf file there for instructions. (Emulation package 9.13.0.00201)
TI UniFlash
Version: 8.5.0.4593
Question: how to flash 2 CC1354 with XDS110 in UNIFLASH software