Part Number: TM4C123GH6PM
#include "tm4c123xx.h"
#include <stdio.h>
#include "uart_header.h"
#define RX_BUFFER_SIZE 1
void delay(long k)
{
while (k--)
;
}
void spi1_config(void)
{
//CLOCK CONFIG
SYSCTL_RCGCSSI_R |= (1 << 1); //CLOCK FOR SPI MODULE 1
SYSCTL_RCGCGPIO_R |= (1 << 3); //CLOCK FOR PORTD
//PD0,PD1,PD2,PD3 CONFIG
GPIO_PORTD_AFSEL_R |= (1 << 0) | (1 << 1) | (1 << 2) | (1 << 3);
GPIO_PORTD_PCTL_R |= (2 << 0) | (2 << 4) | (2 << 8) | (2 << 12);
GPIO_PORTD_DEN_R |= (1 << 0) | (1 << 1) | (1 << 2) | (1 << 3);
/*
SSI1_CR1_R &= ~(1 << 1); // Clearing bit 1 to set CPOL=0 (Clock Polarity)
SSI1_CC_R = 0x0; // SELECTING SYSTEM CLOCK
SSI1_CPSR_R = 40; // Setting CPSDVSR to achieve 125kbps at system clock 16MHz (You may need to adjust this value according to your system clock)
SSI1_CR0_R = 0x07; // SELECT DATA SIZE AS 8BIT AND FRAME AS FREE SCALE FRAME AND SPO AND SPH AS 0 AND SCR AS 0 (This setting corresponds to CPOL=0 and CPHA=0)
SSI1_CR1_R |= (1 << 1); // ENABLE SSI1
*/
}
void spi1_slave(void)
{
SSI1_CR1_R &= (~(1 << 1));
SSI1_CR1_R |= (1 << 2); // SLAVE
SSI1_CR1_R |= (1 << 1);
}
void spi1_master(void)
{
SSI1_CR1_R &= (~(1 << 1));
SSI1_CR1_R &= ~(1 << 2); // MASTER
SSI1_CC_R = 0x0; // SELECTING SYSTEM CLOCK
SSI1_CPSR_R = 40; // Setting CPSDVSR to achieve 125kbps at system clock 16MHz (You may need to adjust this value according to your system clock)
SSI1_CR0_R = 0x07; // SELECT DATA SIZE AS 8BIT AND FRAME AS FREE SCALE FRAME AND SPO AND SPH AS 0 AND SCR AS 0 (This setting corresponds to CPOL=0 and CPHA=0)
SSI1_CR1_R |= (1 << 1);
}
void spi1_write(unsigned char data)
{
while (((SSI1_SR_R >> 1) & 1) == 0)
;
SSI1_DR_R = data;
while (((SSI1_SR_R >> 4) & 1) == 1)
;
}
unsigned char spi1_receive(void)
{
char dt;
while (((SSI1_SR_R >> 3) & 0x1) == 0)
;
dt = SSI1_DR_R;
return dt;
}
void uart5_char_tx(unsigned char data)
{
// Wait for the UART5 transmit FIFO to be not full
while (UART5_FR_R & UART_FR_TXFF)
;
UART5_DR_R = data;
while (tx_flag_5 == 0)
;
}
void uart5_config(void)
{
// CLK_CONFIG
SYSCTL_RCGCUART_R |= (1 << 5); //UART5 PORT CLOCK
SYSCTL_RCGCGPIO_R |= (1 << 4); //GPIO PORTE
//CONFIG PE4,PE5
GPIO_PORTE_AFSEL_R |= (1 << 4) | (1 << 5); //TO SELECT ALTERNATE FUNCTIONS
GPIO_PORTE_PCTL_R |= (1 << 16) | (1 << 20); //SELECTING UART FUNCTION
GPIO_PORTE_DEN_R |= (1 << 4) | (1 << 5); //DIGITIALIZING PE4,PE5
//UART5 CONFIG
UART5_CTL_R &= (~(1 << 0)) & (~(1 << 8)) & (~(1 << 9)); //UART5 DISABLING BEFORE CONFIG
UART5_IBRD_R = 104; //BAUD RATE INTERGER PART
UART5_FBRD_R = 11; //BAUD RATE FRACCTIONAL PART
UART5_LCRH_R |= (0x3 << 5); //WORD LENGTH - 8 BITS
UART5_CC_R = 0x05; //SELECTING POSC
UART5_CTL_R |= (1 << 0) | (1 << 8) | (1 << 9); //0-UART ENABLE,8-TRANSMIT ENABLE,9-RECEIVE ENABLE
}
unsigned char rx_data[RX_BUFFER_SIZE];
int main()
{
spi1_config();
uart5_config();
while (1)
{
spi1_master();
spi1_write('a');
delay(100000);
/*
spi1_slave();
rx_data[0] = spi1_receive();
uart5_char_tx(rx_data[0]);
delay(100000);
*/
}
}
THE COMMENTED LINES INSIDE MAIN. IS IT POSSIBLE FOR THAT TRANSISITION TO HAPPPEN FROM MASTER TO SLAVE. IS THE CODE CORRECT? Please let me know if I am right or wrong.