Other Parts Discussed in Thread: IWR1642, CC2564MODNEM, CC2564
I have IWR1642 BOOST board Evaluation kit. This kit comes with tm4c1294ncdptt3 as xds110 debugger for driving the iwr1642 board. I see tm4c has 20 pin connector in the boar ( You see attached picture ).
Can I use this board to connect with boost em adapter to connect cc2564modnem to use for cc2564 applications. Here, Tm4c129 act as mcu for communication via UART master. I see this tm4c129 can be used for mcu to connect with cc2564 and also sample application code available But I don't know this will be used. Kindly confirm. Please suggest and give some solution and I don't have any other current compatible boards connecting to this cc2564modnem. Whatever in website mentioned boards for cc2564 are obsolete now.