Part Number: TMS570LS0432
In this series i.e TMS5700 i want to communicate with SPI protocol TMS570 with ADXL345 SPI peripheral so please send code and HAL code setting SPI Master Mode with Slave
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LS0432
In this series i.e TMS5700 i want to communicate with SPI protocol TMS570 with ADXL345 SPI peripheral so please send code and HAL code setting SPI Master Mode with Slave
Hi Yogesh,
We don't have any specific tested driver code for "ADXL345".
What we can do is that we can provide example demo codes related to the SPI and based on that you have to write the application code to the "ADXL345"
In below FAQ you can find so many example related to the SPI:

Refer them to understand the basic implementation procedure.
I also found one thread related specific to the ADXL345, here a customer posted his implementation code, you can refer this as well:
--
Thanks & regards,
Jagadish.