Part Number: MSPM0L1306
Other Parts Discussed in Thread: SYSCONFIG
Hi TI!!!
I am new with MSPM0, however I would like to use it in a project.
In my project I need to measure 8 analog signals. Is this possible with the MSPM0L1306?
The MSPM0L1306 has more than 8 pins with analog capability, ok. But CCS allows to select only one pin as analog input.
Am I missing something or do I have to change the analog input pin dynamically in the firmware to read all signals?
What is the best way to read 8 analog signals with the MSPM0L1306?
Thanks very much. Best Regards.