Part Number: TM4C1290NCPDT
Other Parts Discussed in Thread: TPS2052
Hi all,
TivaWare 2.1.4.178
I have a 20MHz crystal and want to run the main system clock at 20MHz but it seems to be running ~25% slower: To get a 10ms SysTick I need to divide the clock frequency by 100 but I have to divide it by 125; to get a UART to run at 9600 baud I have to set it to run at 12,000 baud. I set the clock with:
ClockSpeed = SysCtlClockFreqSet(SYSCTL_USE_OSC | SYSCTL_OSC_MAIN | SYSCTL_XTAL_20MHZ, 20000000); // 20MHz
UARTConfigSetExpClk(UART0_BASE, GetClkSpeed(), 12000,
( UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE ));
SysTickPeriodSet(GetClkSpeed()/125); // Interrupt every 10ms. (convert nS to mS), keep
The crystal is indeed a 20MHz unit, I hope I'm doing something wrong in setting the clock speed.
Thanks